{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Voltage Inputs Burden Rating for ION and Powerlogic Meters

Issue
Burden rating for the voltage input terminals.

Product Line
ION6200, ION75xx, ION76xx, ION86xx, PM5xxx, PM8xxx, PM8xx

Resolution
The voltage input terminals for the Powerlogic and ION meters have a fixed input impedance.
The burden can be calculated thus:

VA per phase = (Input Voltage^2) / (Input impedance)

Kindly refer to the installation guide for your meter's for specifications.
All meter documentation can be found in the Schneider Electric website: http://www.schneider-electric.com

Note for socket meters:
The voltage measurement terminals with the standard power supply options have the same VA rating as the power supply:
20VA max.

The meters with the AUX power supply option measurement terminals have a 5 Mega Ohm input impedance.
For example, if the voltage coming into the terminals is 120V:
V^2/R = 120V^2 / 5Meg =  2.88 x 10^-3 VA per phase.

Schneider Electric Canada

Explore more
Range:
PowerLogic PM5000 seriesPowerLogic ION7550 | ION7650PowerLogic ION8650PowerLogic™ ION9000PowerLogic PM8000 series
Explore more
Range:
PowerLogic PM5000 seriesPowerLogic ION7550 | ION7650PowerLogic ION8650PowerLogic™ ION9000PowerLogic PM8000 series
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.