Search FAQs
What are the Schneider Electric equivalents of Veris Energy Meters?
Environment:
Powerlogic Energy Meter
Resolution:
Veris Part Number | Schneider Part Number |
H8150-0100-0-1 | EMB1-010 |
H8150-0200-0-1 | EMB1-021 |
H8150-0100-0-2 | EMB2-010 |
H8150-0200-1-2 | EMB2-021 |
H8150-0800-3-2 | EMB2-083 |
H8150-0100-0-3 | EMB3-010 |
H8150-0200-1-3 | EMB3-021 |
H8150-0800-3-3 | EMB3-083 |
H8150-0800-4-3 | EMB3-084 |
H8150-1600-4-3 | EMB3-164 |
H8150-0300-2-1 | EMB1-032 |
H8150-0300-2-2 | EMB2-032 |
H8150-0400-3-2 | EMB2-043 |
H8150-0300-2-3 | EMB3-032 |
H8150-0400-3-3 | EMB3-043 |
H8163-0100-0-1 | EME1-010 |
H8163-0200-0-1 | EME1-021 |
H8163-0100-0-2 | EME2-010 |
H8163-0200-1-2 | EME2-021 |
H8163-0800-3-2 | EME2-083 |
H8163-0100-0-3 | EME3-010 |
H8163-0200-1-3 | EME3-021 |
H8163-0800-3-3 | EME3-083 |
H8163-0800-4-3 | EME3-084 |
H8163-1600-4-3 | EME3-164 |
H8163-0300-2-1 | EME1-032 |
H8163-0300-2-2 | EME2-032 |
H8163-0400-3-2 | EME2-043 |
H8163-0300-2-3 | EME3-032 |
H8163-0400-3-3 | EME3-043 |
Released for:Schneider Electric United Arab Emirates
Explore more
Range:
Explore more
Range: