Issue:
Customer wants to configure alarm and event alarms
Product Line:
CM2000 Series Meters
Environment:
Alarm and Event Setpoint Selection
Cause:
The CM2000 series meters has onboard alarms and events that can be configured. There are 4 setpoint settings for each alarm/event: Pickup Value, Pickup Delay, Dropout Value, and Dropout Delay.
The Pickup and Dropout values can be chosen as a certain percent above or below the nominal value for that measurement.
Resolution:
The attached spreadsheet can be used to help determine the desired pickup and dropout values for voltage related alarms/events based on the nominal voltage and the desired pickup and dropout %.
For example, alarm 16 is an overvoltage alarm. If the desired pickup value is 105% of the nominal voltage and the nominal voltage is 480V, the pickup value would be 504V. If the desired dropout value is 95% of the nominal voltage, the dropout voltage would be 456V.
*For information on configuring alarms from the front panel check out Video: Alarm and Relay Setup for the CM2000 Series Meter from the Front Panel
Released for:Schneider Electric United Arab Emirates