The available UL certificate ONLY covers the C60 ranges which belong to the US Multi9 range. The iC60 belongs to the Acti9 range which is not UL certified. If the requirement is to have a multi-standard miniature circuit breaker, then we can offer the global Multi9 multi-standard offer which complies with UL, IEC®, CCC and CSA. This offer is different than the US Multi9 offer.The catalogue for the Multi Standard offer is attached.