{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
Search FAQs
What is the maximum operating voltage for RCD devices ?
As per IEC standards or RCD devices (RCCB with IEC610008 and RCBO with IEC61009), the tolerance is -15% / +10%.

So , if the RCCB has a Un = 400V, it will be operational at 440V max.but taking into consideration that there is no fluctuations in the system voltage as 440V is the maximum voltage it can withstand.

Schneider Electric United Arab Emirates

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.