Search FAQs
Do we have coordination table for GV2 for single pole motor?
So, you could take the rule for selecting the products : According to the nominal motor current ( in single phase ) you select the products ( circuit breaker, contactor, overload protection ) as for a DOL starter with the same nominal current, Kindly find the relevant pages attached.
( Remark : the circuit breaker and the overload relay must be wired with 2 phases in series ) .
You can see in attachment an example of wiring GV2 motor protection circuit breaker for single phase application.
( Remark : the circuit breaker and the overload relay must be wired with 2 phases in series ) .
You can see in attachment an example of wiring GV2 motor protection circuit breaker for single phase application.
Released for:Schneider Electric United Arab Emirates
Attachment(s)
Explore more
Range:
Explore more
Range: