{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.

Search FAQs

CAN NSX AC BREAKER be USED IN DC APPLICATIONS ?

  • ONLY the following 2 categories of the compact NSX AC MCCB are proven to operate under DC rated operatinal voltage as shown in the attached catalogue Panorama.
1- The compact NSX AC MCCB 1 Pole - from 100 to 250A only -  can be used under 250VDC rated operational voltage .
2- The compact NSX AC MCCB 2 Poles - from 100 to 250A only - can be used under 500VDC rated operational voltage.
  • Kindly use the below link to download the Schneider offer for DC networks Circuit breakers from 16 to 4000A Compact NSX DC & Masterpact NW DC.
  • https://www.se.com/uk/en/download/document/LVPED208006EN/

Schneider Electric United Arab Emirates