Search FAQs
What are the operating modes for SFT2841 V14.1 software ?
The SFT2841 V14.1 software is the setting and operating tool for Sepam Series 20, Series 40 and Series 80 relays. It may be used in one of three operating modes.
- Offline mode - prior to commissioning and without connection to the Sepam relay to prepare protection and parameter settings
- Online mode - during commissioning, on a PC connected point-to-point to the Sepam front panel using the CCA783 serial cable: to load, upload and modify Sepam relay protection and parameter settings and to obtain all measurements and useful information during commissioning
- Network mode - during operation, on a PC connected to a set of Sepam relays via an E-LAN multipoint communication network in order to manage the protection system, to monitor the status of the electrical network and to run diagnostics on any incidents affecting the electrical network
Released for:Schneider Electric United Arab Emirates
Explore more
Product:
Explore more
Product: