Search FAQs
Can the M241 PLC be an Ethernet/IP primary?
Issue:
Is the M241 PLC an Ethernet/IP primary?
Product Line:
M241, TM241
Resolution:
Starting with SoMachine V4.3,all M241 controllers an Ethernet IP scanner (primary) capability. That includes Machine Expert 1.x and Machine Expert 2.x versions
Is the M241 PLC an Ethernet/IP primary?
Product Line:
M241, TM241
Resolution:
Starting with SoMachine V4.3,all M241 controllers an Ethernet IP scanner (primary) capability. That includes Machine Expert 1.x and Machine Expert 2.x versions
Released for:Schneider Electric United Arab Emirates
Explore more
Range:
Explore more
Range: