Search FAQs
What is the maximum allowable temperature on the terminals of a Masterpact NW ACB?
Masterpact NW ACBs comply with IEC 60947-2. Temperature rise tests for Masterpact NW ACBs are specified in standard IEC 60947-2. Please find attached a declaration of conformity illustrating the maximum allowable temperature on the terminals of the Masterpact NW ACB.
Released for:Schneider Electric United Arab Emirates
Attachment(s)
Explore more
Range:
Explore more
Range: