{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
Search FAQs
Do we have an interlock for RM6 circuit breaker function that prevents remote operation (motor) while a manual operation is being performed?
In RM6 standard wiring for motorized circuit breaker function, the motor is being interrupted (i.e. not allowed to operate) via dedicated limit switches in case of operation of either the manual hand lever for circuit breaker, the manual hand lever for earthing switch or a locking action.
An example wiring diagram showing the limit switches as below.

Schneider Electric United Arab Emirates