{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
Search FAQs
Does Ecodial comply with IEC 60363 OR IEC 61363 for marine applications design
Ecodial is best suited for Building Application and we do not recommend for Marine applications.
Ecodial follows the following IEC standards
  • IEC 60947 Standards for low-voltage switchgear and controlgear
  • IEC 60364 for installation standard mainly cable installation methods.
  • CENELEC TR50480 for Short circuit calculation.

Schneider Electric United Arab Emirates

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.