{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
Search FAQs
What is the wiring diagram of serial RS232 programming cable for Scadapack 350E RTU ?

This cable is used to connect from an RJ-45-based RS-232 port on the RTU to a DE-9S connector on DTE such as a PC. A 3 m (10 ft.) long cable is available from Schneider Electric using part number TBUM297217.

RJ-45 to DE-9S DTE cable Description

RJ-45
8 Pins

SCADAPack DTE Function

DE-9S DTE Function

DE-9S

Shield connects to shell

6

TxD

RxD

2

5

RxD

TxD

3

4

GND

GND

5

1, 2, 3, 7 and 8 are not connected at this end.

Wires not connected at this end.

Schneider Electric United Arab Emirates