{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.

Search FAQs

What are the authorized losses levels for transformers in EcoDesign regulation EU 548-2014?

For Oil Distribution and Dry-type transformers (≤ 3150 kVA):
  • Losses levels to be applied (reference of MV ≤ 24 kV and LV ≤ 1.1 kV).
  • ODT and CRT not covered by reference transformers (additional losses allowed compared to standard losses ranges):
  • Medium power and power transformers: Level of Peak Efficiency (Mix of load losses and no load losses) for transformers > 3150 kVA (limited to 10 MVA 36 kV for Dry-type Transformers)
- No losses levels imposed but minimum PEI (Peak Efficiency Index)
- PEI corresponds to:
- the maximum efficiency of the transformer
- Ratio between the no load losses and losses

The values given are Maximal value; no more tolerances on design considered:

Schneider Electric United Arab Emirates

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: