Search FAQs
What are the standard rated voltages for medium voltage fuse according to IEC 60282-1? How to properly define its value?
A voltage used in the designation of the fuse-base or fuse-link, from which the test conditions are determined.
The rated voltage of a fuse and should be selected from the following table:
Notes:
The rated voltage of a fuse and should be selected from the following table:
Notes:
- This rated voltage represents the highest voltage for the equipment,
- On three-phase solidly earthed systems, fuses may only be used provided that the highest system voltage is less than or equal to their rated voltage.
- On single phase or non-solidly earthed systems, fuses may only be used provided that the highest system voltage is less than or equal to 87 % of their rated voltage, unless specific testing has been performed
Released for:Schneider Electric United Arab Emirates
Explore more
Category:
Range:
Explore more
Category:
Range: