{}

Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
How can we help you today?
What is the definition of ANSI 81R - Rate of change of frequency?
Protection function used for fast disconnection of a generator or load shedding 
control. Based on the calculation of the frequency variation, it is insensitive to 
transient voltage disturbances and therefore more stable than a phase-shift 
protection function.

Disconnection
In installations with autonomous production means connected to a utility, the “rate of 
change of frequency” protection function is used to detect loss of the main system in 
view of opening the incoming circuit breaker to:
  • protect the generators from a reconnection without checking synchronization
  • avoid supplying loads outside the installation.
Load shedding
The “rate of change of frequency” protection function is used for load shedding in 
combination with the underfrequency protection to:
  • either accelerate shedding in the event of a large overload
  • or inhibit shedding following a sudden drop in frequency due to a problem that should not be solved by shedding.

Schneider Electric United Arab Emirates

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.