{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
Search FAQs
How can I connect Lighting circuits, on/off or dimming, to HRC controllers?

Lighting can be connected to HRC as shown in the following architecture, Consider the following:

  • Lighting on/off control, the use of 230VAC relay is a must.
  • For dimming, the current HRC only supports 0-10V. However, there may be cases of compatibility issues for certain dimming drivers, and therefore, it is recommended to test the compatibility in advance. In case of compatibility issues, adding a resistor (600Ω, 0.5W) in parallel with the dimming drive may solve the issue.

HRC connections

Schneider Electric United Arab Emirates