{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
Search FAQs
I would like to communicate with the ATV320U07M2C series driver and HMIGXU3500 series panel via modbus
Issue:
I can extract all the values from the modbuspoll program with the driver. But when I write a program on the drive, the address I specified in the vijeo designer basic program is over 40001.
eg (9001) the address I want to use. vijeo designer basic program 49002 when I enter this address.
No communication between the drive and the HMI can be achieved.

Cause:
The cause is that the wrong address range checked when writing the M address, it use the word address check instead of bit address check when writing the M512.

Solution:
HotFix Shall be Produced, But we can propose the customer use the "SM" address instead of "M" address as quick workaround.

Schneider Electric United Arab Emirates