{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
Search FAQs
What is the maximum voltage per pole for iC60, C120, NG125 and C60H-DC?

The C60 (or iC60) offers are compliant with 60V DC per pole.
C120 / NG125 offers are compliant with 125V DC by pole
C60H-DC offer is compliant with 250V per pole.

Schneider Electric United Arab Emirates

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: