{}

Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
Search FAQs
Why a 4-20 mA is preferred to 0-10V in analog signals?
The bottom span 4 mA expresses a minimum signal value than a broken wire.
Since the loop current never falls to zero, it can be loop powered, allowing for a two-wire circuit.
20 mA is considered an intrinsically safe signal in most locations.
Elimination of the voltage drop errors results from long wiring runs due to the constant-current feature of a current loop.

Schneider Electric United Arab Emirates

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: