{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.

Search FAQs

What is the difference between In-line and Inside Delta Soft Starter Circuits?

The Altistart 48 connected in the motor supply line

The motor connection depends on the supply voltage, which in this example is a star connection.
1
The motor connection depends on the supply voltage, which in this example is a delta connection.
2

The Altistart 48 connected in the motor delta winding
ATS48***Q or ATS48***YS316 starters connected to motors with delta connections can be inserted in series in the motor windings. They are powered by a current which is less than the line current by a factor of SQRT 3, which enables a starter with a lower rating to be used.

3

Schneider Electric United Arab Emirates

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: