{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
Search FAQs
How to make ENVIRONMENT TEACH MODE for Osiris XUB Photo-electric sensor?
This detector is capable of functioning in all the standard detection modes, i.e.:
Without accessory: Diffuse, Diffuse with background suppression
With accessory: (Reflector or Transmitter): Polarised reflex, Thru-beam
Before performing the ENVIRONMENT TEACH MODE procedure, you must align the detector correctly.
Remove all objects from the detector’s field of detection
Without accessory: place the detector opposite the zone to be detected
With accessory: align the detector on the accessory using the signals provided by the yellow and red LEDs (Yellow LED on and Red LED off signals
correct alignment).
You have aligned the detector and it is now ready for the ENVIRONMENT TEACH MODE procedure. To do this:
- Remove all objects from the detector’s field of detection
- Press in and hold the «teach» pushbutton.
- The green LED goes out then comes on again after about 3 seconds.
- Release the «teach» pushbutton when it comes on
- The green LED flashes to indicate that environment teaching is in progress. Then
- If the green LED comes on, the detector has been taught the environment and is ready to function.
- The detection mode (Diffuse, Diffuse with background suppression, Polarised reflex, Thru-beam) is memorized, and the INITIAL SETTING can only be restored by performing a RESET
- Any object passing within its detection field (in front of a background or between the detector and the reflector or transmitter) will be detected; the Yellow LED comes on and the output is activated.
If the red LED starts flashing very rapidly, the environment teaching procedure has failed:
- The detector may be misaligned
- An object passed within its detection field during teaching
- The background or the reflector is too close to the detector
- Readjust the alignment conditions, perform a RESET 6°) then repeat the ENVIRONMENT TEACH MODE procedure.

Schneider Electric United Arab Emirates

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: