{}

Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
How can we help you today?
What is the function of USB ports of SmartX IP controller devices?
Issue:
Need to know the function of SmartX IP controller devices USB ports

Product Line:
EcoStruxture Building Operation, SmartX IP controller devices

Resolution:

1. MP Series controllers, and IP-IO modules:
MP Seriescontrollers, MP-C, MP-V, and IP-IO modules, have two USB ports, host and device ports. These ports are reserved for future use
.
2. RP Series controllers:
RP Series controllers have two USB ports, host and device port.
The USB host port is a USB 2.0 type-A port, which is rated 2.5 W. The USB host port can be used for connection of the Smart Zigbee Adapter to add Zigbee TM wireless connectivity to the RP-C controller, requires EBO V3.2 or higher and RP-C firmware V3.0.2.01 or higher. The Smart Zigbee Adapter can be used to extend the controller's point count and bring flexibility in retrofit applications. 

The USB device port is a USB 2.0 mini-B port. The USB device port is reserved for future use.

Schneider Electric United Arab Emirates

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.