{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
Search FAQs
Whether daisy chain of Easergy P3 relay with 2 x RJ-45 Ethernet ports work properly or not ? & What is maximum no. device we can connect ?
Issue:
Easergy P3 relays with 2 x RJ-45 Ethernet ports.

Environment/Product line:
Easergy P3 relay.

Resolution:
Yes ,the daisy chain of Easergy P3 relays with 2 x RJ-45 Ethernet ports should work, up to a maximum of 10 devices.

Schneider Electric United Arab Emirates