Search FAQs
Using Pick Action For "Change Main Server" Action
This Pick Action can be used to switch between servers for users without database permission. This is useful for administrators who wants to keep the Main server as Main after a failover. With the use of a button and a click, it will provide you with options to select the server of your choice.
- Create a new mimic and create a button from the Graphical tab in ViewX.
- Double click the button to display “Button Properties” dialog.
- Click the “Pick Action” button.
- From the Pick action configuration, select “Method” and click “Next”
- Click the ellipsis on the right and locate root explorer.
- Beside “Method” select from the drop-down list “Change Main Server” and click “Next”.
- Click “Next” button twice and “Finish”.
- Save changes and place in “Run Mode”.