Issue:
Can I monitor Analog Input signals on ATV212 display?
Product Line:
ATV21, ATV212
Environment:
All
Cause:
Want to confirm analog input signal strength wired to VFD.
Resolution:
It is not possible to monitor the VIA or VIB signal values on the HMI display.
Released for:Schneider Electric United Arab Emirates