{}

Our Brands

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.
Search FAQs
Can a Model 6 MCC be configured to 415VAC 50Hz voltage system?

415v 50hz is available for Model 6 MCC's as a special. We can issue special pricing for the application. Will have to know if there are any control power transformers or power supplies that will need to be converted.

Schneider Electric United Arab Emirates

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: