Leakage current from APC Back UPS products
Issue:

How can I gauge the amount of leakage current from my Back-UPS?

Product Line:

All Back-UPS models.

Environment:

N/A

Cause / Resolution:

All APC Back UPS models, by themselves exhibit less than 1 milli-amps of leakage current. If a load is attached, then the leakage current measured on the output of the UPS will include the leakage current of the load as well as the UPS.

Example:
Load 1 has measured leakage current of 2millli-amp
Load 2 has measured leakage current of 1milli-amp
UPS  has measured leakage current of 0.5milli-amp

Therefore, the total leakage current that can be measured from the UPS input should be 2+2+.5 = 4.5milli-amp


Schneider Electric Argentina

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: