Can you change the cycle time on an InRow ACRD100, ACRD200, ACRP100, ACRD500?
Issue:
Can you change the cycle time on an InRow ACRD100, ACRD200, ACRP100, ACRD500?

Product line:
InRow DX

Environment:
Data Center Cooling

Cause:

Resolution:
The unit cannot operate in Lead/Lag mode under InRow operations. You will have to select HACS,RACS or Spot allowing you to access operational screen to configure Lead/Lag.

Runtime balancing can be enabled through the following path: Configure Group->Runtm Bal. When enabled the controls will shuffle primary and backup roles of units periodically to balance the system run-time of the units in the group.

Runtime balance is 72 hours.  Please note that this does not mean that the units will switch every 72 hours.  This means that the units will switch when there is 72 hours of runtime difference between the units.This is not changeable.

Schneider Electric Argentina

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: