AirFlow CCT CW to DX Change Over

Article available in these languages: Spanish

Issue:
AirFlow CCT CW to DX Change Over

Product line:
Airflow

Environment:
Data Center Cooling

Cause:

Resolution:
In the event there is a need to run a Legacy Airflow product (CCT, or TC) in direct expansion (DX) mode while shutting down or doing maintenance on the chilled water (CW) system, below is the proper way to do a CW temp switch over.

Temp >> Down Arrow >> Down Arrow >> [You should see FreeCool: ECWS] >> Set the FreeCool OFF mode below the current water temp.  This will cause the compressor(s) to come on as long as there is a demand for cooling.

NOTE: Attached are documents regarding External Chilled Water Supply (ECWS) and its operation.
NOTE: These instructions are for a DG5.0 controller.

Schneider Electric Argentina

Documentos adjuntos
DG5.0 DX with ECWS Setup Instructions rev. 20111013.pdf [780.72 KB]
DG 5 Microprocessor Controller O and M Manual.pdf [215.98 KB]
Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: