Where can I find basic programming information for ATV312 drives?
Issue:
Programming information for ATV312?

Product line:
Altivar ATV312

Environment:
All models, all serial numbers

Cause:
Basic Programming for the ATV312 drive.

Resolution:
drC Menu
Parameter setting  Description
bFr   Standard Motor frequency  (50Hz or 60Hz depending on the motor and power system)
UnS   Rated Motor Voltage
FrS   Rated Motor Frequency (usually matches bFr)
nCr   Rated Motor Current  (nameplate current for the motor at the voltage it's being used)
nSP   Rated Motor Speed  (nameplate RPM for the motor at the frequency it's being used)
tFr   Max Frequency
uFt   Motor control type (defaults to n; Sensorless Vector Control, some applications work better at L; Standard V/Hz)

SET Menu
ACC   Acceleration
dEC   Deceleration
LSP   Low Speed
HSP   High Speed
ItH   Motor Thermal  (set to the motor nameplate current for the voltage being used, provides Overload protection) ItH should = nCr
uFr   Voltage boost  (usually can be left at default)
CLI   Current limitation  (sets peak current allowed to go to the motor.  If set too low, can prevent the motor from reaching the commanded speed; display will flash off and on)

IO Menu
tCC    2/3 wire type  (default is 2C; 2 wire control) [must hold Enter for 2 seconds when changing]
tCt   2 wire type  (default is trn; drive must see the transition (off to on) of the run command to start the motor.)  Some applications require this to be changed to LEL. Review the installation to be sure this is safe.
rrS   Reverse assign (default is LI2)
When in 2C (2 wire control), LI1 is the Run Forward input.
When in 3C (3 wire control), LI1 is a Stop input, LI2 is Run Forward and LI3 is Run Reverse.

CtL menu
LAC= L1, L2 or L3 (default is L1, L2 and L3 activate advanced functions in the drive) [must hold Enter for 2 seconds when changing]
Fr1= Sets where the speed reference comes from.  Default is AI1 (0-10VDC) Other options are AI2, AI3, A1U1, UPdt, UPdh, LCC, Ndb or nEt
or
Fr2= Sets where the secondary speed reference comes from.  Active only if Reference Switching (rFC is used)
Cd1= Sets where your run command comes from. Options are [Terminal], [Local], [Remot. HMI], [Modbus], and [Com. Card]. (Parameter can be accessed if [Profile] (CHCF) = [Separate] (SEP), and [ACCESS LEVEL] (LAC) =(L3).)
CHCF= (SIM or SEP) Sets whether your run command and speed reference come from the same source or separate sources

Examples
AI1= speed pot  0-10vdc input
AI2= -10 +10vdc  analog input
AI3= 4-20mA analog input
A1U1= Local speed knob on the face of the drive
UPdt= +/- Speeds
UPdh= +/- Speeds via the remove HMI
LCC= Local mode
ndb= Modbus reference
nEt=  reference via network communications protocol.

Refer to the ATV312 Programming Manual for additional information.

https://www.se.com/ww/en/download/document/BBV46385/

Schneider Electric Argentina

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: