Issue
Which events can be triggered from an either an input contact or output relay on the AP9613 Dry Contact Relay I/O SmartSlot Card?
Product Line
- UPS Device Management
- AP9613 Dry Contact I/O SmartSlot Card
- AP9335T/TH Environmental Sensors
- AP9810 Dry Contact I/O Accessory Dongle
Environment
- All firmware versions
- All serial numbers
Cause
General information - if a user is interested in which events can be mapped to an input contact or output relay on the AP9613, refer to the list below. Legacy Configuration options (those available with the older AP9610 SmartSlotCard) are available via dip switch configuration (outlined in the user's guide) or also as a template in the configuration utility the AP9613 offers.
If you would like to customize which inputs or outputs map to which commands and/or relay numbers, please refer to the user's guide for the AP9613 in using the "Custom" dip switch configuration in order to utilize the Dry Contact I/O SmartSlot Card Configuration Utility to do the customization.
Resolution
The available targets on the standalone AP9613 for input contacts include:
- UPS
- UPS Outlet Group 1*
- UPS Outlet Group 2*
- UPS Outlet Group 3*
- Output Relay 1
- Output Relay 2
- Output Relay 3
- Output Relay 4
- Output Relay 5
- Output Relay 6
- UIO Port 1 Output Relay (if optional AP9810 is connected)
- UIO Port 2 Output Relay (if optional AP9810 is connected)
If you choose the UPS or an Outlet Group as the target, the following (control) Actions are available:
- On
- On With Delay
- Off
- Off Gracefully
- Shutdown
- Shutdown with Delay (With outlet groups only)
- Reboot
- Reboot Gracefully
- Self Test (Not available with outlet group target)
- Bypass* (Not available with outlet group target)
The available events on the standalone AP9613 for output relays include:
- On
- Off
- Online
- On Battery
- On Battery: Power Fail
- Low Battery
- Replace Battery
- Lost Communication
- Overload
- Bypass: Fault or Software*
- Bypass: Manual or Software*
- Bypass: Manual
- Off or Lost Communication
- Self Test
- Calibration
- Self-test Fail
- Fault (AP9613 Dry Contact I/O SmartSlot Card "Legacy Fault" Definition for more information)
- Fault Legacy 1 (AP9613 Dry Contact I/O SmartSlot Card "Legacy Fault" Definition for more information)
- Fault Legacy 2 (AP9613 Dry Contact I/O SmartSlot Card "Legacy Fault" Definition for more information)
- Fault Legacy 3 (AP9613 Dry Contact I/O SmartSlot Card "Legacy Fault" Definition for more information)
- Mains Out of Tolerance
- Bypass Out of Tolerance*
- Output Out of Tolerance
- No battery
- Battery Over Temperature
- Input Breaker Tripped
As an added option and for expansion, the AP9613 has (2) Universal I/O ports that support the following accessories:
- AP9335T or AP9335TH Temperature or Temperature and Humidity Sensors
- AP9810 Dry Contact I/O Accessory
With the optional AP9335T or AP9335TH Environmental Sensors, the following alarms can be configured:
- Temperature Above Maximum
- Temperature Below Minimum
- Humidity Above Maximum
- Humidity Below Minimum
These environmental alarms as well as the inputs from the optional AP9810 Dry Contact I/O Accessory Dongle can then be mapped to one of the following targets:
- UPS
- UPS Outlet Group 1*
- UPS Outlet Group 2*
- UPS Outlet Group 3*
- Output Relay 1
- Output Relay 2
- Output Relay 3
- Output Relay 4
- Output Relay 5
- Output Relay 6
- UIO Port 1 Output Relay (if optional AP9810 is connected)
- UIO Port 2 Output Relay (if optional AP9810 is connected)
If you choose the UPS or an Outlet Group as the target, the following (control) Actions are available:
- On
- On With Delay
- Off
- Off Gracefully
- Shutdown
- Shutdown with Delay (With outlet groups only)
- Reboot
- Reboot Gracefully
- Self Test (Not available with outlet group target)
- Bypass* (Not available with outlet group target)
If you choose an Output Relay as a target, the following Actions are available:
- Abnormal
- Normal
Publicado para:Schneider Electric Argentina