APC Home - How to Create Schedules
Issue:
How to create a schedule on the APC Home App

Resolution:
Follow the instructions below:
  1. Open APC Home App.
  2. Tap Schedules.
  3. Click the + icon.
  4. Enter Schedule Name.
  5. Tap "Add outlets from" to select outlets.
  6. Select the outlets and when finished tap the back icon.
  7. Tap the days of the week to set the time and days of the schedule.
  8. Select Action: Turn outlets on or off.
  9. Select Time and select either AM or PM.
  10. Select the days for the schedule to be performed and when finished tap the back icon.
  11. Tap Save.

Schneider Electric Argentina

Documentos adjuntos
APC Home - How to Create a Schedule.mkv [8.26 MB]
Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: