How to set sensitivity for BVX series 700VA , 900VA, 1200VA, 1600VA, 2200VA?
Issue:
How to set sensitivity for BVX series?

Product Line:
Back-UPS models beginning with BVX

Environment:
All models specified above, All Serial Numbers

Cause:
There are times that the sensitivity settings need to be changed due to the actual condition of the main source/utility in order to keep the UPS operation smooth and normal.


Resolution:

Servlet


Voltage Sensitivity Adjustment
Press and hold the power On/Off  button for 10 seconds until a beep is heard. The LED will flash and sensitivity LOW is set.
If press and hold the power On/Off button for 10 seconds again, the LED will be On and sensitivity MEDIUM is set.
Capture.JPG

Schneider Electric Argentina

Explora más
Producto:
Explora más
Producto: