Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Schneider Electric Makes eConversion the Default Mode for its Galaxy V-Series UPSs

Sydney NSW, Australia

29/11/2022

  • eConversion mode offers a three-times reduction in Uninterruptible Power Supply (UPS) electricity consumption with 99% efficiency without compromising availability  
  • eConversion has been certified to achieve Class-1 protection per IEC® 62040-3, which is the maximum level and matches Double Conversion 
  • Schneider Electric continues to prove its sustainability leadership by being the first manufacturer to deploy 3-phase UPSs in high-efficiency mode as the default protection 

Schneider Electric™, a global leader in the digital transformation of energy management and automation, announced an enhanced version of eConversion (formerly known as ECOnversion), the company’s generally-recommended protection mode to provide increased sustainability for its Galaxy V Series 3-phase UPSs. After years of field tests, effective May 31, 2022, all Galaxy V Series UPSs will be shipped to customers with eConversion as the default. 

With cost of ownership and sustainability as an ongoing pain point, Schneider Electric is the only company that offers this unique, patented combination of performance and efficiency. eConversion mode provides the highest protection level for critical loads with Class-1 (UL certified) and results in savings up to three times the UPS price. Providing critical back-up power solutions for IT and non-IT environments, such as industrial edge applications, Galaxy V Series’ eConversion delivers reliable power protection and helps attain new levels of sustainability.

eConversion has over eight years of field deployment and thousands of customers worldwide who use it daily to protect their critical loads since its launch in 2014. 

“With eConversion as the default mode for Galaxy V Series 3-phase UPSs, we expect to facilitate the conservation of 175 GWH of electricity annually – which is the equivalent of the energy produced by nearly 60000 rooftop solar installations.” Says Mustafa Demirkol, Vice President of Data Centre Systems, Offer Management and Marketing, Energy Management at Schneider Electric. “We’re looking forward to helping customers meet their sustainability goals while reducing their electricity spending and corresponding carbon emissions.”

High Efficiency Mode Mitigates Impact of Rising Energy Costs

According to the World Bank, energy prices are expected to rise more than 50 percent in 2022 before easing in 2023 and 2024. Utilising eConversion enables operators to mitigate some of the cost and climate impact while continuing to benefit from the highest protection level for critical loads with Class-1 (UL certified). And with the eConversion Savings Meter, customers can check electricity savings on the UPS display.

Customers can still choose to use the legacy Double Conversion mode, but field experience has shown that modern electrical installations do not justify such high permanent use of electricity. EcoDataCentre, a climate-positive HPC data centre, deployed four Galaxy VX UPSs at 1250 kW each to support customer loads with the possibility to run at 99% efficiency with eConversion mode.

As digital demand will continue to grow and require resilience to reap the benefits of automation and efficiency, data centre, OT, and IT professionals will need to make step-changes towards a net-zero world. eConversion is available as a feature in all Galaxy V Series UPSs worldwide.

Adoption of Wiztopic's Blockchain Certification Platform

From 2nd October 2019, in order to secure its communication, Schneider Electric has been certifying its content on Wiztrust. You can check the authenticity on the website Wiztrust.com for corporate communications.
View press release (pdf, 185 kb) opens in new window
Share this page: