{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

What is the approximate weight of a typical Model 6 LVMCC section?

Issue:
What is the approximate weight of a typical Model 6 LVMCC section?

Product Line:
Model 6 motor control centers.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The following weights are approximate shipping weights for a normal mix of LVMCC equipment. Some sections, based on installed devices and width of section may vary from the weights shown.

NEMA 1, 1A, & 12 Enclosure, 15 inches deep - 600 lbs
NEMA 3R Non-Walk-In Enclosure, 15 inches deep - 900 lbs

NEMA 1, 1A, & 12 Enclosure, 20 inches deep - 750 lbs
NEMA 3R Non-Walk-In Enclosure, 20 inches deep - 1050 lbs


CTA-ID : 2005295

Schneider Electric Australia