{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the difference between a shunt trip and shunt close device on a Masterpact breaker?
Issue:
What is the difference between a shunt trip and shunt close module on a Masterpact NW or NT breaker?

Product Line:
Power circuit breakers

Resolution:
There is no difference in the accessory and they are marked to be used as either. Their function is determined by which position they occupy in the breaker. When used as a shunt trip, the coil trips the breaker when the rated voltage (Vn) is applied. When used as a shunt close, the coil closes the breaker when Vn is applied as long as there is nothing preventing the breaker from closing (an open command, the open button being pressed, and engaged padlock attachment, etc.) See attached instruction bulletin 48049-146-01 for more information.

Schneider Electric Australia

Attachment(s)
MX MN 48049-146-01.pdf [161.17 KB]