{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are the dimensions and weights of the ATS48C21Y, ATS48C25Y and ATS48C32Y?
Issue:
Dimensions and weights of ATS48C21Y, C25Y and C32Y

Product Line:
ATS48C21Y, ATS48C25Y and ATS48C32Y

Environment:
Dimensions and weight

Cause:
N/A

Resolution:
Width = 12.6 inches (320 mm)
Height = 14.96 inches (380 mm)
Depth = 10.43 inches (265 mm)
The weight is 40.1 pounds (18.2 kg)

Schneider Electric Australia