{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the part number for the replacement coil for the CA2SK11 relays?
Issue:
Replacement coil for the CA2SK11 relay.

Product Line:
TeSys SK IEC Style Relays

Environment:
IEC Style Industrial Control Relays

Cause:
Clarify if there's a replacement coil or if entire relay must be replaced.

Resolution:
Coil is not a replaceable part. Replace the entire relay.

Schneider Electric Australia