{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are the coil voltage codes for the LC1D115 / LC2D115 and LC1D150 / LC2D150 TeSys contactor?
Issue:
LC1D115-150 Coil voltages options

Product Line:
Contactors and Starters-IEC

Environment:
Tesys D Contactors

Resolution:
The following list the more common voltage suffix codes for these product lines.  For a more comprehensive list and to determine compatibility with a given product, refer to the catalog below.

Note 1: LC1D150 contactors are only available with *7 coil codes.
Note 2: Coil Code ending number represents frequency rating as follows:
5 = 50 Hertz
6 = 60 Hertz
7 = 50/60 Hertz

AC Volts ___Code                DC Volts ___Code
24 ___ B5 or B6 or B7          12 ___ Not Avail.
42 ___ D5 or D7                   24 ___ BD
48 ___ E5 or E6 or E7          36 ___ CD
110 ___ F5 or F6 or F7         48 ___ ED
115 ___ FE5 or FE7             60 ___ ND
120 ___ G6 or G7                72 ___ SD
127 ___ FC5 or FC7            110 ___ FD
208 ___ L6 or LE7               125 ___ GD
220 ___ M5 or M6 or M7       220 ___ MD
230 ___ P5 or P7                 250 ___ UD
240 ___ U5 or U6 or U7        440 ___ RD
277 ___ W6 or UE7
380 ___ Q5 or Q6 or Q7
400 ___ V5 or V7
415 ___ N5 or N7
440 ___ R5 or R6 or R7
480 ___ T6 or T7
500 ___ S5 or S7


Schneider Electric Australia