{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

Can additional contact blocks be stacked on 9001K35H2 joystick?

Issue:
How many contact block can be added on the 9001K35H2 joystick?

Product Line:
Push buttons and operator Interface

Environment:
9001, 9001K35, KA1, Joystick

Cause:
Additional contact blocks are needed for application.

Answer:
A maximum of 2 more contact blocks can be added. If (2) 9001KA1`s are added, there will be (2) contacts that close in each position (excluding the OFF position).

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: