{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the ampere rating for dc voltages for the 9001KA contact blocks?
Issue:
DC ampere rating for 9001KA contact blocks

Product Line:
9001K 30mm Push Buttons

Environment:
Harmony 30mm Operators

Resolution:
2.5A continuous up to moved. (NEMA Q600)

Schneider Electric Australia