{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

What is EUSERC and what does it mean?

Issue:
Acronym meaning

Product Line:
Metering Equipment

Resolution:
EUSERC is an acronym for electric utility service equipment requirements committee. Formed in 1983, the purpose of the organization is to promote uniform electric service requirements among the member utilities, publish existing utility service requirements for electric service equipment, and provide direction for development of future metering technology. There are approximately 80 utilities involved in EUSERC from 12 states. Not all EUSERC member utilities accept all metering devices that meet EUSERC specifications. So, although a device may meet EUSERC specifications, it may not be accepted for use by a specific utility company. Always check with the utility company for approval before using any metering device.

NOTE: NOT ALL OF THE SQUARE D METERING EQUIPMENT WILL MEET EUSERC, BECAUSE EUSERC HAS CERTAIN REQUIREMENTS, FOR EXAMPLE, THEY USE RING TYPE METERS AND NOT ALL METERS ARE RING TYPE. CHECK WITH THE LOCAL UTILITY COMPANY FOR APPROVAL BEFORE USING ANY METERING DEVICE.

Schneider Electric Australia