{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are the mounting restrictions for the U-Line starter ?
Issue:
Identify the mounting positions for U line starter

Product Line:
Tesys U Open Motor starters and Protectors

Environment:
IEC Style Contactors and Starters

Resolution:
The devices are limited to a tilt (front to back) of no more than 30 degrees from vertical and sideways of no more than 90 degrees to the left or the right.


Schneider Electric Australia