Issue:
Contact Rating of 9013F Pressure Switches
Product Line:
Pressure, vacuum and Float Switches
Environment:
9013 Type F Pressure Switch
Resolution:
Those contacts have a control circuit rating of A600.
They are DC rated at 1/4 HP at 115V and 230V (Except form M4)
They are Single Phase AC rated 1 1/2 HP at 115V, 2 HP at 230V
They are Polyphase rated 2 HP at 115V, 3 HP at 230V, and 1 HP at 460/575V.
This also applies to the 9013 FHG2, 9, 12, 13, 44, 49 9013 FSG, and FSW.
Contact Rating of 9013F Pressure Switches
Product Line:
Pressure, vacuum and Float Switches
Environment:
9013 Type F Pressure Switch
Resolution:
Those contacts have a control circuit rating of A600.
They are DC rated at 1/4 HP at 115V and 230V (Except form M4)
They are Single Phase AC rated 1 1/2 HP at 115V, 2 HP at 230V
They are Polyphase rated 2 HP at 115V, 3 HP at 230V, and 1 HP at 460/575V.
This also applies to the 9013 FHG2, 9, 12, 13, 44, 49 9013 FSG, and FSW.
Released for:Schneider Electric Australia