{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the power terminal lug data for the LC1D40, LC1D50, LC1D65, LP1D40, LP1D50, and LP1D65 contactor?
Issue:
Identifying power terminal lug data for the D2 style contactors

Product Line:
IEC Contactors and Starters

Environment:
Tesys D line contactors

Cause:
Power terminal lug data required

Resolution:
For contactors with screw clamp terminals:
stranded cable w/o cable end : One #10-3 AWG or Two #10-4 AWG per terminal.
stranded cable w/cable end: One #10-4 AWG or Two #12-2 AWG per terminal.
solid cable: One #10-3 AWG or Two #10-6 AWG per terminal.

Schneider Electric Australia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.