Issue:
What Padlock Device can be used on the 9001KR9R E-stop Pushbutton?
Product Line:
30 mm push buttons
Environment:
Harmony 30 mm 9001 SK Plastic Push Buttons
Resolution:
9001K62, 9001K162
NOTE: These attachments will not work when the operator is supplied with a 2 1/4 inch diameter mushroom.
What Padlock Device can be used on the 9001KR9R E-stop Pushbutton?
Product Line:
30 mm push buttons
Environment:
Harmony 30 mm 9001 SK Plastic Push Buttons
Resolution:
9001K62, 9001K162
NOTE: These attachments will not work when the operator is supplied with a 2 1/4 inch diameter mushroom.