{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Are the ZB2 and ZB4 operators interchangeable?
Issue:
Verifying the ZB2 and ZB4 compatibility

Product Line:
Push Buttons and Operator Interface

Environment:
ZB4/ ZB5 22mm Harmony Push Buttons

Cause:
Determine if the existing ZB2 unit has to be completely replaced, or replacement parts are available.

Resolution:
No, the ZB2 operators can’t be used with the ZB4 contacts and light modules and the ZB4 operators cannot be used with the ZB2 contacts and light modules. The lines are both 22mm so the complete devices can be substituted.

Schneider Electric Australia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.