{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How can we help you today?

What the DC current contact ratings for the CAD50, CAD32, CAD503, CAD323, CAD506, and CAD326 relay?

Issue:
Checking on the DC current contact ratings for the CAD50, CAD32, CAD503,  CAD323,  CAD506, and  CAD326 relay.

Product Line:
CAD Industrial Relays

Environment:
Relays and Timers

Resolution:
Inductive:
125V DC - 0.55 Amps make and break, 2.5 Amps cont.
250V DC - 0.27 Amps make and break, 2.5 amps cont.
600V DC - 0.10 Amps make and break, 2.5 Amps cont.

Schneider Electric Australia