{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is meant by common trip as it relates to a 2 or 3 pole breaker?
Issue:
Does a handle switch trip both breakers?
Product Line:
Miniature Circuit Breaker
Resolution:
This means the 2 or 3 poles are linked internally and if any pole trips, they all open together.
Single pole breakers linked externally with a handle tie are not common trip. One breaker (pole) tripping does not trip the others.

Schneider Electric Australia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.